2020-01-27 09:50 PM
Hello I am trying to use Touch GFX. In CubeMX I installed the related software pack:
When I open the additional software part there is no option I can enable Touch GFX, it is simply empty:
How can I enable it from CubeMX? Thank you beforehand.
Solved! Go to Solution.
2020-04-20 12:47 AM
Thanks Martin, 🙂
so in this case can you tell me if there is an "easy" way of putting the TouchGFX on the H747 disco?
2020-04-20 12:57 AM
Well i think it's easy, but it's definitely not as easy as using TouchGFX Generator + CubeMX :D
Just to get you started - I think you should read the TouchGFX Generator documentation to see how it sets up a Touchgfx project, and you just do the same. Start by checking out the H743 AT from the designer and copy the touchgfx relevant files to your own project. Start by doing some inspection and let me know.
/Martin
2020-04-20 02:15 AM
Ok thanks for the tip will need to do some additional reading in spare time 🙂
thanks for the time being for your help
BR Pawel