cancel
Showing results for 
Search instead for 
Did you mean: 

Touch GFX additional software window is empty

GunkutA
Senior

Hello I am trying to use Touch GFX. In CubeMX I installed the related software pack:

0690X00000Bwig6QAB.png

When I open the additional software part there is no option I can enable Touch GFX, it is simply empty:0690X00000Bwig1QAB.png

How can I enable it from CubeMX? Thank you beforehand.

12 REPLIES 12

Thanks Martin, :)

so in this case can you tell me if there is an "easy" way of putting the TouchGFX on the H747 disco?

Well i think it's easy, but it's definitely not as easy as using TouchGFX Generator + CubeMX :D

Just to get you started - I think you should read the TouchGFX Generator documentation to see how it sets up a Touchgfx project, and you just do the same. Start by checking out the H743 AT from the designer and copy the touchgfx relevant files to your own project. Start by doing some inspection and let me know.

/Martin

Ok thanks for the tip will need to do some additional reading in spare time :)

thanks for the time being for your help

BR Pawel