cancel
Showing results for 
Search instead for 
Did you mean: 

Text configuration in VisualStudio

Marco.R
Senior

Hi

In the TouchGFX Designer is it possible to set the text configuration to "Remap texts" and "A4" and it works well when I'm generating the code.

But when I build within VisualStudio these settings will not applied, even they are added within the "application.config" file.

Has anyone an idea where the problem can be?

/Marco

3 REPLIES 3
Martin KJELDSEN
Chief III

I just to verify, but i think this is a bug that we just fixed for 4.14.0

/Martin

Sounds good. When will 4.14. be available?

/Marco

​Week 31 :)