2024-02-27 07:04 PM
Hello. Recently I received an STM32U5G9J-DK2 board which I purchased earlier this year. I want to ask for the Out-of-Box Demo of this board for backup since I find it really stunning and I want some reference for my own TouchGFX GUI application design. So, where should I go for asking? Or is this demo available in source project or binary file or neither makes sense? Can I, as a student, be able to get a binary file version of it?
Looking forward to your replies. Thanks in advance.
Solved! Go to Solution.
2024-03-14 08:05 AM
Yes, the demos are a bit different. We cannot share that project with you, but I can send you the binary file
Good luck
2024-02-28 06:10 AM
Hello @Nathan_Xi ,
The OBD for STM32U5G9J-DK2 is based on the TouchGFX Demo 7 that is available on TouchGFX Designer. And, you can access the source code as well.
I hope this answers your question.
2024-03-07 03:55 AM
Err...thank you but I suppose that it's not the same demo software however, the original one has a vector map subdemo and a animated vector font subdemo. That's apparently not the same. Is there an original version of that?
2024-03-14 08:05 AM
2024-03-28 12:44 AM
Thank you so much!I always expected that a binary file could be given. This really proves to be a good "solution" to this blog.
2024-04-02 12:16 AM
You're very welcome!
2024-08-24 09:34 AM
Thanks for providing the demo file.
I have tried to use STM32CubeProgrammer to flash it to my STM32U5G9J-DK2 board, but met with an error (shown below) during programming as shown in the screenshot below:
I could never get flashing and verification to complete successfully - I would either meet with programming errors once progress reached segment 1, or verification errors.
I am not familiar with the procedure of flashing a binary which contains both internal and external flash segments. I presume its failing to write to the external flash memory?
Could you please help provide the instructions for reflashing the DevKit board with the OBD?
2024-08-28 04:52 AM
Hello @vinkwok,
Have you tried erasing the full chip flash memory, and the flashing the board using External Flash Loader?
If the error persists, please create a new thread on the forum.
Best regards,
2024-11-06 02:35 PM
I'm in similar situation. I purchased the STM32U5G9J-DK2 and was very impressed with the built-in demo.
I then used CubeMX and CubeIDE to port some simple code from a 32F429 project to verify the migration.
It worked with very few changes required!
However, now I want to show off the Demo program to a colleague so they can see how good the graphics looks.
But I cannot find any way to restore the original demo program.
If possible, please send me the Binary file or Hex File so I can restore the board to when I first received it.
Thanks,
David
2024-12-02 04:03 PM
Hello. You can find the binary file in the accepted solution.
Just download it.
Best wishes.