2019-01-17 12:44 PM
Working on getting a new TFT DSI LCD display to work on the STM32L4R9I-DISCOVERY kit. It uses the ST7796H2 display driver. emWin shows they have added support for this in their 5.36 version in the GUIDRV_FlexColor files, but STemWin is only reved to 5.32.
TouchGFX doesn't use the GUIDRV_FlexColor, where are the hardware specific files for editing to add support for this new LCD? I've read: (https://touchgfx.zendesk.com/hc/en-us/articles/204993942-Changing-to-a-different-display) but it doesn't mention specific file and I've browsed through various files without noticing the right one to work with. (GuiConfig.h, gui_main.h/cpp, stm32l4xx_hal_lcd.h, ...)
Thanks for your guidance and support.
2019-01-23 1:56 PM
Review the DSI document from Qualcomm that is attached. Specifically table 3-1 and see if it helps. Keeping in mind that DSI registers are supposed to be common across any vendor of the display, review the horizontal values to see if they impact your display. This is exciting as it appears that you are getting closer!
2019-01-23 1:59 PM
Also this thread:
2019-01-23 2:05 PM
Thanks a lot Mon! I'll make sure to review that doc and link you shared.
2019-01-23 9:13 PM
2019-01-23 9:14 PM
2019-01-23 9:16 PM
2019-01-27 7:01 AM
Good job @Du !! Thank you for posting. We are planning to use a 800x480 IPS with CTP and DSI interface in the near future. Will be performing a similar exercise as the controllers are changing with the wind direction. Details to follow after that review. Hope to review some displays at the upcoming fairs in HK (April).
2019-01-27 4:56 PM
Thanks @Mon2 ! Good luck with your project! Looking forward to hearing about it.