cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7B3I with appwizard GUI using Keil, can not build project?

MHana.1
Associate III

Hello, I am using STM32H7B3I development kit and with appwizard generating the UI for the board using Keil MDK-ARM V5.24.1, I can not find the suitable library and if I linked any given library i still has many errors that can not be resolved especially undefined symbol.

Is there any ready project to try AppWiazrd with Keil for STM32?

1 REPLY 1
KDJEM.1
ST Employee

Hello @MHana.1 ,

 

To increase the probably of obtaining a answer, could you please share your project and errors screenshot?

May this post can help you.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.