2021-09-07 2:26 AM
Since upgrading from 4.15 I've not been able to create new blank projects or any of the examples when selecting by board. The error message is: "Combination of STM32H7B3I & Blank UI failed" for the blank example the version is v 3.0.7 which appears to be the most recent.
2021-10-06 6:40 AM
Hi Romain, I tried a few things but really needed an installed setup that others can also use, so I ended up rolling back to designer 4.15.0 and have continued to work with that. Probably easiest (for me anyway) is to retry another update when you next release one (and possibly on a clean PC too) to see what happens. Thanks for the update, Martin.