cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743zit DCMI DMA not Working.

SSche.1
Associate II

I can not get the DCMI Working with OV7670 Camera.

The Hardware is correct, Camera setup is correct.

 HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_CONTINUOUS, (uint32_t)framebuffer, sizeof(framebuffer)/4);

The DMA Always Fails.

The problem is with the STM32Cube generated code.

I need to help debugging the Problem.

Who can I discuss the problem with?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Dub Bartolec
Senior

What is the memory area you are trying to DMA it to ?

Not all memory areas on STM32H7 can be accessed by the DMA.

What is the address of "frambuffer" in above code snippet ?

SSche.1
Associate II

DBart.1

uint16_t *framebuffer = ( uint16_t *)0x24000000 ; // AXI SRAM @ 0x0x24000000 -0x2407FFFF (512 KByte) in domain D1

uint32_t frambuffer_size = 320*240*2 ; // Bytes

SSche.1
Associate II

Is there anyone at STMicro that can confirm and Fix the Bugs in the STM32Cube for STM32H743zit code.

Please send me the contact Info. I'll help in anyway I can.