cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7508-DK : Blank screen after flashing TouchGFX GUI

Woula
Associate II

Hi,

I am trying to flash a single screen Touch GFX application on my STM32F7508-DK board but I got a blank screen.

Did anyone face that problem before ? What could be the solution ?

My actual configuration:

TouchGFX Designer 4.21.0

Thanks in advance!

3 REPLIES 3
Karl Yamashita
Principal

Do you mean the STM32H750B-DK? Did you press the black reset button? I'm working on this board this very minute. Unlike other TouchGFX projects, this one does not start after being programmed from STM32CubeIDE until you reset it.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

No. I think they are different.

I did press the reset button many times but nothing had changed.

Even the examples are not displayed after being flashed. The screen remains blank.

Have you've checked to see if the External Loaders section has a memory device selected?

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.