cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F479VI MIPI-DSI interfacing with PI camera

ZTale.1
Associate II

hello

i am designing a custom board and i need to interface a PI camera with MIPI-DSI interface.

i need to know if the video data provided by the PI-camera is handled by the STM32F479VI MIPI-DSI interface.

regards.

Zakaria

1 REPLY 1
AWEI.2
ST Employee

MIPI-DSI is for the display interface, can't be used in the camera part. the camera is using the MIPI-CSI interface, now ST MP1 is supporting the interface.