2025-01-24 05:53 AM - last edited on 2025-01-24 06:23 AM by SofLit
I have designed a STM32F429 Custom TFT Board With 4.3" TFT it is based on 32F429IDISCOVERY MCU + RAM + 4.3" TFT in 16 bit mode and I'm using TouchGFX.
I have few questions.
1) It is possible to remove External RAM from the System.
2) How to limit RAM Usage so as to use the internal MCU RAM only
2025-01-24 06:15 AM
Hello,
Are you using TouchGFX for this case?
2025-01-24 06:17 AM
Hello,
Yes, I am using the Touchgfx.
2025-01-24 06:22 AM - edited 2025-01-24 06:24 AM
Ok. Need to tell that in the first post because the answer may differ and your question could be generic not specific (related to TouchGFX).
I'm editing it then ..
2025-01-24 06:30 AM
I did specified that " I have designed a STM32F429 Custom TFT Board With 4.3" TFT it is based on 32F429IDISCOVERY MCU + RAM + 4.3" TFT in 16 bit mode and I'm using TouchGFX ".
I would like to know your thoughts on using internal RAM as Frame buffer.
2025-01-24 06:34 AM - edited 2025-01-24 06:39 AM
@Caan wrote:
I did specified that " I have designed a STM32F429 Custom TFT Board With 4.3" TFT it is based on 32F429IDISCOVERY MCU + RAM + 4.3" TFT in 16 bit mode and I'm using TouchGFX ".
No. That was my edit ;)
One of the TouchGFX expert can help you on that.
2025-01-24 07:43 AM
Alright, Thank you for the help.
2025-01-27 06:12 AM
No Response till now!