Hello @KMew (Community Member)
Here below my answer to your previous questions:
"The level I'm looking at (ADC_Display) does not match what's in the project explorer. "
Again, that's is normal because STM32CubeIDE as a configuration view of it's root folder that is STM32CubeIDE\
"I went into one of the subfolders (ADC_Display/STM32CubeIDE) and I found a matching file directory!"
Yes and that is what I already explain to you yesterday and just above.
"Now, it still poses an issue because this project folder is missing things like the header files and such. Does this information help at all? The .project and .cproject should be in the ADC_Display folder, not ADC_Display/STM32CubeIDE folder, correct?"
No your project generated has no issue. All sources and header file are located on folder above \STM32CubeIDE, like ..\Core or ..\TouchGFX.
Yes these informations are mandatory and STM32CubeIDE is able to found them because the path of the project are correctly configured (see following picture)
These folder path configuration are also into the .cproject file.
I confim again there is no issue in your generated project.
Best regards
Romain