2019-04-30 12:24 PM
Hello
I am using the STM32F769-Disco Board with Touchgfx and CubeMX (and Atollic True Studio). I am not getting it working with the following manual: https://touchgfx.zendesk.com/hc/en-us/articles/360020208091-Configuring-STM32F769I-DISCO
Can someone help me?
I've got the STM32F746-Disco running with parallel-RGB interface. The STM32769-Disco has a DSI interface and I do not know what I've done wrong or if the manual has some issues.
Dejan
2019-05-03 02:37 AM
Hi. Have not tested this target yet but the above referenced article details a procedure using the IAR compiler.
Are you using the IAR compiler?
2019-05-08 06:53 AM
I am using Atollic True Studio.
When I am setting up the project with STM32CubeMX then I can't get the display working with TouchGFX.