STemWIN does not work on STM32L4R9-DISCO
I'm trying to start the Hello World application and the application generates HardFalut when calling the function GUI_DispStringHCenterAt. While debugging it seem that within the library function GUI__GetLineDistX a call to null pointer function happens. As i can see the third parameter stored at r2 points to a non populated function and jump to 0x0000000 happens.
Stack call thread is:
Thread #1 (Suspended : Signal : SIGINT:Interrupt)
HardFault_Handler() at stm32l4xx_it.c:67 0x800056e
<signal handler called>() at 0xfffffff9
0x0
GUI__GetLineDistX() at 0x800c7b2
GUI_DispString() at 0x80073ec
GUI_DispStringHCenterAt() at 0x80074f4
MainTask() at BASIC_HelloWorld.c:25 0x8000286
main() at main.c:102 0x800038c
I've noticed this behavior in using System workbench and import of examples from:
STM32Cube_FW_L4_V1.14.0 and then PATCHED to 1.15.0
STM32Cube_FW_L4_V1.16.0
STM32Cube_master (from github version 15 with latest STemWIN downloaded from STM)
Is there any possible cause that is already known?