STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Exit from QSPI Memory map mode in STM32H7

Hi Guys,I am working on one of the project, in that I have to read the TouchGFX assets from External flash and also sensor data from external flash.So, TouchGFX assets has to be read in Memory Map Mode and Sensor data has to be read in Indirect Mode....

AMull.11 by Associate II
  • 1078 Views
  • 0 replies
  • 0 kudos

Resolved! STM32 F746G-DISCO

Hello there, I am actually new in coding STM32 boards. I am currently working on an STM32 F746G-DISCO. i am using the "LCD_UsrLog ((char *)" to print messages on the LCD tft screen. I am wondering if there some high level function that enables me to ...

WBen .2 by Associate II
  • 1581 Views
  • 2 replies
  • 1 kudos

Resolved! Image widget drawing issue while Box widgets are ok

I'm working on a project based on STM32F769ii MCU with external Flash via Qaud-SPI and 480x800 DSI LCD(no onboard GRAM). I have successfully integrated TouchGFX into my project however I see unexpected artefacts with the image widgets. Box widgets ar...

KT by Associate II
  • 6660 Views
  • 8 replies
  • 0 kudos

Resolved! LTDC Interface wiring STM32F429I-DISCO.

Hi All,I am trying to work out wiring for my discovery board with an ILI9488 TFT Display (MIPI-DBI 16 bit) and as I was going through Discovery board schematics for reference.  I checked the default board configuration in STM32CubeMx but the RGB565 (...

0693W00000AM0kNQAT.png 0693W00000AM0i3QAD.png 0693W00000AM0urQAD.png
PKara.1 by Associate II
  • 1761 Views
  • 1 replies
  • 0 kudos

Emulator support for STM32l4R9 Series ICs.

Hi, For a new project, We have our custom board with STM32L4R9ZI IC. In our hardware setup, we don't have an external RAM to use Double Buffer. So we are using Single Buffer for rendering purpose. we have our UI with transitions like Carousel, Cover...

generating the 3 colored palette

I'm trying a palette that goes from white to red and red to green. Following this article https://support.touchgfx.com/docs/development/ui-development/scenarios/creating-dynamic-l8-images, I could make the columns colored. But I couldn't make it 3 co...

0693W000008zxJaQAI.png
Ezgi by Senior
  • 1435 Views
  • 4 replies
  • 0 kudos