2019-04-09 9:36 PM
I am trying to integrate STM32CubeMX and TouchGFX using IAR EW on STM32F769I-Discovery Board. I followed the instructions on the link below to configure the board:
https://touchgfx.zendesk.com/hc/en-us/articles/360020208091
Then, I use ST-link Utility to program my board following the steps given in:
But, ST-link Utility is unable to program the external memory and throws 'File out of External Memory Range' error and does not shows 0x90000000 as an external memory when hex file is opened in ST-link.
I have successfully implemented Embedded Wizard's demo program on the board but stuck with TouchGFX!
2019-04-09 11:46 PM
Hi @HKaur,
If you select V2.0.0 of the STM32F769-DISCO application template from the designer you should be able to program your board.
That article you're linking to exists to compensate for errors in CubeMX generation. I will remove it soon because as CubeMX improves TouchGFX code and project generation these articles lose their purpose.
The work has already been done for you in the F769-DISCO application template.
Check it out and let me know!
Best regards,
Martin
2019-04-10 1:52 AM
I am configuring the STM32F769I discovery Board in CubeMX and then use 'Execute' to generate the TouchGFXdesigner application.
But I think , TouchGFX doesn't maps the target correctly from CubeMX as the 'Run Target' option is inactive. (highlighted in yellow) Though it generates code without an error.
How can I select V2.0.0 of the STMF769-DISCO in the TouchGFX designer now?
2019-04-10 5:08 AM
2019-04-10 5:12 AM
Use the STM32 Cube Programmer, it replaced the ST-LINK Utilities. Make sure you pick the External Loader for your board, the search line allows you to declutter the list.
2019-04-10 10:23 PM
Hi Martin,
Thank you for the quick reply.
This option to select the application template is available when I start creating my project in TouchGFX. But when I start in CubeMX and 'Execute' it from CubeMX, The TouchGFX designer automatically opens up but there is no option available to choose the application template from this route.
Also, if I wish to use Keil UVision (most of my team members are currently using Keil), is there an option to generate the Keil Project in TouchGFX for STM32F769I-DISCO?
2023-12-30 5:59 AM - edited 2023-12-30 6:17 AM
Your tip actually worked! Thanks!