cancel
Showing results for 
Search instead for 
Did you mean: 

Skip check of the build targets once the simulator.exe is linked

ferro
Lead

Hi,

every time I press 'Run Simulator', the build system checks all targets if update is needed. This takes often up to 10s.

0693W00000Y98nUQAR.pngIs there any way to run immediately simulator.exe ?

Thanks

5 REPLIES 5
Smartembedded
Associate III

You could find and run the simulator.exe directly from the build dir ?

Yes, I could. Thanks.

Is there a way to run it from within TouchGFX generator ? Is there a way to customize Generator e.g. adding a button to execute ceratin task ?

Do you mean the generator embedded into CubeMX ?

If yes, it is not possible to run the simulator from there, it is only used to generate code in your project depending on the configuration you chose.

Yoann KLEIN
ST Software Developer | TouchGFX

"Do you mean the generator embedded into CubeMX ?"

I see, sorry for the confusion. I meant from the tool "TouchGFX designer".

ferro
Lead

Not exactly what I am looking for but good to know that pressing F5 restarts the simulation.

However, F5 does not resets C++ program data.

keyboard-shortcuts