Skip to main content
TWebs.1
Associate II
November 9, 2019
Solved

Simulator error after including header files in Model.cpp

  • November 9, 2019
  • 1 reply
  • 1180 views

Adding the following includes in Model.cpp prevents the touchgfx simulator from successfully compiling:

#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
 
extern "C"
{
#include "main.h"
#include "FreeRTOS.h"
#include "queue.h"
#include "task.h"
}

I tried adding to the makefile include path as follows, but I think I'm going down a rabbit hole.

#keep framework include and source out of this $(build_root_path)../Core/Inc
include_paths := $(library_includes) $(foreach comp, $(all_components), $(comp)/include) $(framework_includes) \
C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Core/Inc \
C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Drivers/STM32F7xx_HAL_Driver/Inc \
C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Drivers/CMSIS/Device/ST/STM32F7xx/Include
source_paths = $(foreach comp, $(all_components), $(comp)/src) $(framework_source) simulator

The simulator errors:

 Compile

    make -f simulator/gcc/Makefile -j10

    Converting images

    Compiling gui/src/model/Model.cpp

    In file included from C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Drivers/STM32F7xx_HAL_Driver/Inc/stm32f7xx_hal_def.h:30:0,

             from C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Drivers/STM32F7xx_HAL_Driver/Inc/stm32f7xx_hal_rcc.h:29,

             from C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Core/Inc/stm32f7xx_hal_conf.h:231,

             from C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Drivers/STM32F7xx_HAL_Driver/Inc/stm32f7xx_hal.h:30,

             from C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Core/Inc/main.h:31,

             from gui/src/model/Model.cpp:8:

    C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Drivers/CMSIS/Device/ST/STM32F7xx/Include/stm32f7xx.h:162:3: error: #error "Please select first the target STM32F7xx device used in your application (in stm32f7xx.h file)"

     #error "Please select first the target STM32F7xx device used in your application (in stm32f7xx.h file)"

      ^~~~~

    In file included from gui/src/model/Model.cpp:8:0:

    C:/Users/webst/STM32CubeIDE/workspace_1.0.1/stm32F769I_disco_cubeide/Core/Inc/main.h:33:22: fatal error: otm8009a.h: No such file or directory

     #include "otm8009a.h"

               ^

    compilation terminated.

Any suggestions? My project in cubeide compiles fine, but I'd like to maintain the ability to use the simulator.

This topic has been closed for replies.
Best answer by TWebs.1

Found the example on the website that shows the correct way:

#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
 
#ifndef SIMULATOR
extern "C"
{
#include "main.h"
}
#include "FreeRTOS.h"
#include "queue.h"
#include "task.h"
extern osMessageQId displayMessageQHandle;
extern osMessageQId displayMessageQ2Handle;
uint8_t newEncoderCount = 0;	//this is the variable local to this file that the message queue populates in the model tick when received
static uint8_t ucLEDState = FALSE;
#else
#define FALSE	0
#define TRUE	1
#endif
 
 
Model::Model() : modelListener(0)
{
 
}
 
void Model::tick()
{
#ifndef SIMULATOR
	if (xQueueReceive(displayMessageQHandle, &newEncoderCount, 0) == pdTRUE)
	{
		modelListener->setEncoderCount(newEncoderCount);	//takes the value out of the queue and lets the listener know so that it can call the function
													//that informs the presenter which then updates the view
	}
#endif
}
 
void Model::getLEDState()
{
#ifndef SIMULATOR
 if (ucLEDState == FALSE)
 {
 	ucLEDState = TRUE;
 }
 else
 {
 	ucLEDState = FALSE;
 }
	xQueueSend(displayMessageQ2Handle,&ucLEDState,0);
#endif
}
 

1 reply

TWebs.1
TWebs.1AuthorBest answer
Associate II
November 10, 2019

Found the example on the website that shows the correct way:

#include <gui/model/Model.hpp>
#include <gui/model/ModelListener.hpp>
 
#ifndef SIMULATOR
extern "C"
{
#include "main.h"
}
#include "FreeRTOS.h"
#include "queue.h"
#include "task.h"
extern osMessageQId displayMessageQHandle;
extern osMessageQId displayMessageQ2Handle;
uint8_t newEncoderCount = 0;	//this is the variable local to this file that the message queue populates in the model tick when received
static uint8_t ucLEDState = FALSE;
#else
#define FALSE	0
#define TRUE	1
#endif
 
 
Model::Model() : modelListener(0)
{
 
}
 
void Model::tick()
{
#ifndef SIMULATOR
	if (xQueueReceive(displayMessageQHandle, &newEncoderCount, 0) == pdTRUE)
	{
		modelListener->setEncoderCount(newEncoderCount);	//takes the value out of the queue and lets the listener know so that it can call the function
													//that informs the presenter which then updates the view
	}
#endif
}
 
void Model::getLEDState()
{
#ifndef SIMULATOR
 if (ucLEDState == FALSE)
 {
 	ucLEDState = TRUE;
 }
 else
 {
 	ucLEDState = FALSE;
 }
	xQueueSend(displayMessageQ2Handle,&ucLEDState,0);
#endif
}