2022-02-24 10:43 AM
Hello everyone,
I am trying to make an LM020L work in Proteus. I am using Eclipse to code.
I am trying to follow the datasheet for the initialization of the LCD and set the cursor at the beginning. This is where I found info: https://web.alfredstate.edu/faculty/weimandn/lcd/lcd_initialization/lcd_initialization_index.html
I want to use 4-bit mode.
Here is my current code:
void resetlcd(void){
GPIOB->BSRR &= ~(GPIO_BSRR_BS9); //RS
GPIOB->BSRR &= ~(GPIO_BSRR_BS10); //RW
GPIOB->BSRR &= ~(GPIO_BSRR_BS11); //E
GPIOB->BSRR &= ~(GPIO_BSRR_BS12); //D4
GPIOB->BSRR &= ~(GPIO_BSRR_BS13); //D5
GPIOB->BSRR &= ~(GPIO_BSRR_BS14); //D6
GPIOB->BSRR &= ~(GPIO_BSRR_BS15); //D7
GPIOB->BSRR |= (GPIO_BSRR_BR9);
GPIOB->BSRR |= (GPIO_BSRR_BR10);
GPIOB->BSRR |= (GPIO_BSRR_BR11);
GPIOB->BSRR |= (GPIO_BSRR_BR12);
GPIOB->BSRR |= (GPIO_BSRR_BR13);
GPIOB->BSRR |= (GPIO_BSRR_BR14);
GPIOB->BSRR |= (GPIO_BSRR_BR15);
}
void LCD_Init(void){
// Ukljuciti takt za dati Port -> Enable the peripheral clock of GPIO Port X
RCC->APB2ENR |= RCC_APB2ENR_IOPBEN; // Enable the peripheral clock of GPIO Port C
GPIOB->CRH &= ~(GPIO_CRH_MODE9 | GPIO_CRH_CNF9); // delete settings for PB9
GPIOB->CRH |= (GPIO_CRH_MODE9_1 | GPIO_CRH_CNF9_0); //GPO Push-pull
GPIOB->CRH &= ~(GPIO_CRH_MODE10 | GPIO_CRH_CNF10); // delete settings for PB10
GPIOB->CRH |= (GPIO_CRH_MODE10_1 | GPIO_CRH_CNF10_0); //GPO Push-pull
GPIOB->CRH &= ~(GPIO_CRH_MODE11 | GPIO_CRH_CNF11); // delete settings for PB11
GPIOB->CRH |= (GPIO_CRH_MODE11_1 | GPIO_CRH_CNF11_0); //GPO Push-pull
GPIOB->CRH &= ~(GPIO_CRH_MODE12 | GPIO_CRH_CNF12); //delete settings for PB12
GPIOB->CRH |= (GPIO_CRH_MODE12_1 | GPIO_CRH_CNF12_0); //GPO Push-pull
GPIOB->CRH &= ~(GPIO_CRH_MODE13 | GPIO_CRH_CNF13); // brisemo podesavanja za PB13
GPIOB->CRH |= (GPIO_CRH_MODE13_1 | GPIO_CRH_CNF13_0); //GPO Push-pull
GPIOB->CRH &= ~(GPIO_CRH_MODE14 | GPIO_CRH_CNF14); // brisemo podesavanja za PB14
GPIOB->CRH |= (GPIO_CRH_MODE14_1 | GPIO_CRH_CNF14_0); //GPO Push-pull
GPIOB->CRH &= ~(GPIO_CRH_MODE15 | GPIO_CRH_CNF15); // delete settings for PB15
GPIOB->CRH |= (GPIO_CRH_MODE15_1 | GPIO_CRH_CNF15_0); //GPO Push-pull
delay(20000); // turning on
resetlcd();
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(30000);
GPIOB->BSRR |= (GPIO_BSRR_BS12);
GPIOB->BSRR |= (GPIO_BSRR_BS13);
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS12);
GPIOB->BSRR |= (GPIO_BSRR_BS13);
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS12); //DB4
GPIOB->BSRR |= (GPIO_BSRR_BS13); //DB5
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS13); //DB5
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS13); //DB5
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
//dsp off
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS15); //DB7
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
//dsp on
resetlcd();
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
GPIOB->BSRR |= (GPIO_BSRR_BS12); //DB4
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(10000);
//entry mode set
resetlcd();
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
resetlcd();
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS11); // enable
delay(10000);
GPIOB->BSRR |= (GPIO_BSRR_BS12); //DB4
GPIOB->BSRR |= (GPIO_BSRR_BS13); //DB5
GPIOB->BSRR |= (GPIO_BSRR_BS14); //DB6
GPIOB->BSRR &= ~(GPIO_BSRR_BR11); // disable
delay(100000);
resetlcd();
}
Can anybody tell what went wrong? Also, I would appreciate it if someone can help me to write a simple "Hello world" message, that is my goal but I am currently stuck on the initialization.
2022-02-25 8:48 AM
Yes. First wrong step is to post code without informations about results (how you know that code is wrong).
Few highlits about writing your own driver fro HD44780.
Be sure that you are using right IO voltages (5V powered display does not have to read 3.3V levels). Use 3.3V powered LCD or use Open drain outputs at 5V tolerant pins of your STM and dont forget add pullup on display enable pin.
Be sure that you set contrast to acceptable level. With wrong level you can fall in situation when display works but you simply cant see it.
Be sure that your SW realize right delay times in first part of communication when you can't read busy bit.
Double check connections.
Best way is to adapt some working library. Sending my own in attachment if you want to use ... written for STM32F0. Can be easily adapted to STM32F1 if you modify GPIO init.
2022-02-25 9:57 AM
Thank you for sharing the library! I found some libraries online I managed to modify some of them in order of my use case. I will post it here once I make it work.
Thank you again!