ScrollWheel UpdateItemCallbackHandler Not Firing After Nth Element
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-12 7:33 AM
Windows 10, TouchGFX Designer 4.17.0, STM32CubeIDE 1.6.1, Simulator (STM32F469 Disco board present).
What I'm trying to do:
I'm creating a ScrollWheel - manually, without TouchGFX Designer. I use auto-generated ScrollWheel code from Base.cpp as a base code for my own element in View.cpp so that I can customize stuff the way I want (generated on another screen - I just needed pieces of auto-generated code as a base for my code).
In View.cpp (and hpp), I have manually created ScrollWheel with one custom container (no special container for the selected item). The custom container itself is pre-created in Designer, I only link my own scrollwheel to that custom container (attempts at creating custom container outside TouchGFX Designer failed). Then I add callback and whatnot. And it even kinda works correctly (code coming).
What goes wrong:
What's interesting is that my ScrollWheel's update item callback function is only called while I scroll between 0-6th elements out of 0-9 elements (=touchgfx_print inside callbackhandler writing stuff). If I drag the scrollwheel so that element 7 (or 8 or 9) is in the "Selected" position, the callback handler doesn't fire, doesn't do printf and other stuff. Only between elements 0-6 it works flawlessly.
Clearly something happens around element 6, but I don't understand what.
Here's some code, how I created the monster that I created:
View.cpp:
void ScreenMeasurementsView::generatePickProgramWheel() {
pickProgramScrollWheel.initialize();
for (int i = 0; i < pickProgramScrollWheelListItems.getNumberOfDrawables(); i++) {
pickProgramScrollWheelListItems[i].initialize();
}
pickProgramScrollWheel.setPosition(210, 215, 190, 170);
pickProgramScrollWheel.setHorizontal(false);
pickProgramScrollWheel.setCircular(false);
pickProgramScrollWheel.setEasingEquation(touchgfx::EasingEquations::backEaseOut);
pickProgramScrollWheel.setSwipeAcceleration(5);
pickProgramScrollWheel.setDragAcceleration(5);
pickProgramScrollWheel.setNumberOfItems(10);
pickProgramScrollWheel.setSelectedItemOffset(-5);
pickProgramScrollWheel.setDrawableSize(50, 5);
pickProgramScrollWheel.setDrawables(pickProgramScrollWheelListItems, updateItemCallback);
pickProgramScrollWheel.animateToItem(0, 0);
add(pickProgramScrollWheel);
}
void ScreenMeasurementsView::updateItemCallbackHandler(touchgfx::DrawableListItemsInterface *items, int16_t containerIndex, int16_t itemIndex) {
if (items == &pickProgramScrollWheelListItems) {
touchgfx::Drawable *d = items->getDrawable(containerIndex);
pickProgramCContainer *cc = (pickProgramCContainer*) d;
pickProgramScrollWheelUpdateItem(*cc, itemIndex);
cc->setNumber(itemIndex);
//cc->setNumber(pickProgramScrollWheel.getSelectedItem());
for(int i=0;i<10000;i++);
Unicode::snprintf(selectProgramTextAreaBuffer, WILDCARD_BUFFER_MAX_SIZE, "%d", pickProgramScrollWheel.getSelectedItem());
selectProgramTextArea.resizeToCurrentText();
selectProgramTextArea.invalidate();
//osDelay();
touchgfx_printf("Current item: %d\n", pickProgramScrollWheel.getSelectedItem());
}
}
Here I create my scrollwheel. Also, every time an item is updated, I also set setNumber - which simply writes the number of every element into dummy elements (its name and code stolen from TouchGFX documentation on ScrollWheel, modified, removed icon changing part) - and does it correctly - my elements initially don't have text ("WC_1WC_2" is its initial content to be accurate, two wildcards with buffers), this function writes stuff to their wildcard buffers correcty, even to elements that I can't select, what I see in simulator is "Program 0", "Program 1"..."Program 9" (all numbered correctly). Also, I write selected item's number into a separate independently created textArea next to my scrollwheel. And I do touchgfx_printf with the selected item number too. It's these numbers that have problems crossing "6" (and showing 7, 8 or 9).
Because the callback doesn't get called when I have 6 or larger selected.
In the element custom container, I actually don't have a textArea, I create it manually in pickProgramCContainer.cpp like this:
void pickProgramCContainer::generateTextAreaW2WC() {
programNameTextArea.setXY(0, 0);
programNameTextArea.setPosition(0, 12, 190, 50);
programNameTextArea.setColor(touchgfx::Color::getColorFromRGB(255, 247, 20));
programNameTextArea.setLinespacing(0);
touchgfx::Unicode::snprintf(programNameTextAreaBuffer1[0], WILDCARD_BUFFER_MAX_SIZE, "WC_1");
programNameTextArea.setWildcard1(programNameTextAreaBuffer1[0]);
touchgfx::Unicode::snprintf(programNameTextAreaBuffer2[0], WILDCARD_BUFFER_MAX_SIZE, "WC_2");
programNameTextArea.setWildcard2(programNameTextAreaBuffer2[0]);
//programNameTextArea.resizeToCurrentText();
programNameTextArea.setTypedText(touchgfx::TypedText(T_TAHOMA_BOLD_20_CENTER_2WC_RESOURCE));
add(programNameTextArea);
}
Obviously, whatever needs to be created in header files, is created (variables for wildcard buffers, textarea itself etc). But then again, the text inside elements actually is correct for all elements. I don't think the problem is connected with this textArea-in-the-container part of the code.
Also, all callbacks are hooked up. Duh, otherwise they wouldn't work for the first elements:
ScreenMeasurementsView::ScreenMeasurementsView() :
WAIT_TIMER_TICKS(0), buttonCallbackView(this, &ScreenMeasurementsView::buttonCallbackHandlerView), flexButtonCallbackView(this, &ScreenMeasurementsView::flexButtonCallbackHandlerView), updateItemCallback(
this, &ScreenMeasurementsView::updateItemCallbackHandler) {
}
WAIT-bla-bla is my custom function, which I'm not using atm, doesn't do anything, not relevant here.
Also, in View.HPP, this is how scrollWheel is declared
touchgfx::ScrollWheel pickProgramScrollWheel;
touchgfx::DrawableListItems<pickProgramCContainer, 64> pickProgramScrollWheelListItems;
As far as I have figured, that "64" means the number of elements that are simultaneously visible. I tried 2, I tried 4, I tried 64. When 2, I only see 2 elements at a time on screen. When more than 2, I see 3 (more don't fit in the scrollwheel anyway). This number didn't affect callback firing behavior.
If you want to see some other pieces of code, you're welcome to ask, I do realize my presentation of my situation can be a little chaotic, also given its unusual nature. Can't post entire file as a single View.cpp already has over 400 lines of code, mostly creating different containers and textareas, and they all work OK and they're completely independent from this piece, but if you really ask, I will create a new empty screen and try to reproduce the problem without unnecessary and/or unrelated stuff.
- Labels:
-
STM32F4 Series
-
TouchGFX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-13 5:54 PM
Hello ilyus,
Implementing a ScrollWheel by code should be definitely possible.
I see that the problem is not related to a board, so could you enclose a UI only project ? (in order to make things easier and having a small enough zip file)
To do so, create a new project as Blank UI and then click Edit -> Import UI -> Select the correct .touchgfx of your project with F469-DISCO and validate.
If you don't understand what I just said, just send me your current project and I'll do the isolation myself.
/Alexandre
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-20 8:00 AM
Of course, will do tomorrow. However, the screens in TouchGFX where I generate stuff are all blank/almost blank anyway, I create EVERYTHING with code only. But sure, instructions seem simple. Guess I'll send you both things. (the project moved on since then, but I was working on another screen, the problem with only elements 0-6 reacting and 7-9 noy is still there)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-21 7:06 AM
Barely got to it. Have a million things at a time at work. Zipped up the whole touchGFX project folder, figured it will quicker. I had no time/opportunity to extract UI. But then again, all my screens are almost blank anyway.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-21 9:53 PM
Hello ilyus,
After some investigation, I fixed the issue. Actually, you were not using the ScrollWheel correctly. I attached the fixed project.
Since I modified a lot of things, it's complicated to explain it here so I wrote 'STMicro" a bit everywhere to help you see what I changed.
If you have any questions about the code, please write them in this post and try to be as precise as possible :)
I highly recommend you to take a look at the ScrollWheel ScrollList UI example available in TouchGFX Designer. I helped myself with it to fix your issue.
In the future, when a problem is related to UI implementation, please isolate the problem by creating a dedicated project for it. In fact, it takes a lot of time and efforts to go through code that is not necessary for fixing the issue.
If everything is fine for you, please close this topic by choosing Select as Best.
/Alexandre