2025-01-20 08:55 AM
I want to create a scrollWheel that has 3 preset options. Option A, Option B, and Option A&B
The issue I have is that I can never get itemIndex = 1 in scrollWheelUpdateItem callback , only index 0 and 2. Also, after I first change wheel, it takes a while to be able to change it again.
I tried to provide all the relevant code and touchgfx setup.
Appreciate if you can tell me what is incorrect.
Here is my Container (MenuItem):
Here is how I set up my text:
scrollWheel:
Here is Container MenuItem.cpp:
#include <gui/containers/MenuItem.hpp>
#include <texts/TextKeysAndLanguages.hpp>
#include <BitmapDatabase.hpp>
MenuItem::MenuItem()
{
}
void MenuItem::initialize()
{
MenuItemBase::initialize();
}
void MenuItem::setWheelElements(int item)
{
switch (item)
{
case 0:
text.invalidate();
text.setTypedText(TypedText(T_S1));
break;
case 1:
text.invalidate();
text.setTypedText(TypedText(T_S2));
break;
case 2:
text.invalidate();
text.setTypedText(TypedText(T_S3));
break;
}
}
MenuItem.hpp:
#ifndef MENUITEM_HPP
#define MENUITEM_HPP
#include <gui_generated/containers/MenuItemBase.hpp>
class MenuItem : public MenuItemBase
{
public:
MenuItem();
virtual ~MenuItem() {}
virtual void initialize();
void setWheelElements(int item);
protected:
};
#endif // MENUITEM_HPP
Buttons1MenuView.cpp
#include <gui/buttons1menu_screen/Buttons1MenuView.hpp>
#include <gui_generated/common/FrontendApplicationBase.hpp>
#include "config_file.h"
#include "math.h"
Buttons1MenuView::Buttons1MenuView()
{
}
void Buttons1MenuView::setupScreen()
{
Buttons1MenuViewBase::setupScreen();
}
void Buttons1MenuView::tearDownScreen()
{
Buttons1MenuViewBase::tearDownScreen();
}
void Buttons1MenuView::scrollWheelUpdateItem(MenuItem& item, int16_t itemIndex)
{
scrollWheel.invalidate(); //NOT SURE IF NEEDED
item.setWheelElements(itemIndex);
}
Buttons1MenuView.hpp
#ifndef BUTTONS1MENUVIEW_HPP
#define BUTTONS1MENUVIEW_HPP
#include <gui_generated/buttons1menu_screen/Buttons1MenuViewBase.hpp>
#include <gui/buttons1menu_screen/Buttons1MenuPresenter.hpp>
class Buttons1MenuView : public Buttons1MenuViewBase
{
public:
Buttons1MenuView();
virtual ~Buttons1MenuView() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void scrollWheelUpdateItem(MenuItem& item, int16_t itemIndex);
protected:
};
#endif // BUTTONS1MENUVIEW_HPP
Solved! Go to Solution.
2025-02-03 07:14 AM
I missed that, thank you!
2025-01-20 09:45 AM
I increased the size of the scrollWheel window (still making it only show one item) it responds much better and I do now get valid itemIndex, accept the index number does agree to what I thought it should be.
In other words, I assume Option A should have index 0, Option B index 1 and Option AB index 2,
but I get Option A index 1, Option B index 2 and Option AB index 0
Anyone know why the indexes as not as expected?
2025-01-21 02:37 AM
Hello @FJB2069 ,
Getting the "right" index when using a scrollWheel is tricky.
This is because it is not meant to be accessed. Instead, the scrollWheel should be used as a menu selector to navigate through your application or to select various options.
Therefore, you should only use the 2 callbacks provided setitempressedcallback and setitemselectedcallback .
So in a way I am avoiding your question because this is not how you should use the scrollWheel and I invite you to not use the index but only the 2 callbacks if you can.
If you really want to use the index of the elements, you should use the scrollList.
I hope this helps.
Regards,
2025-01-21 07:37 AM - edited 2025-01-21 10:21 AM
I changed from a scrollWheel to a scrollList. I get exact same results.
1) How might I implement setitemselectedcallback in my existing code?
I tried below, but will not trigger?
2) Also, I need to initialize the scrollList. How can I do this in Buttons1MenuView::setupScreen()?
Buttons1MenuView.hpp
#ifndef BUTTONS1MENUVIEW_HPP
#define BUTTONS1MENUVIEW_HPP
#include <gui_generated/buttons1menu_screen/Buttons1MenuViewBase.hpp>
#include <gui/buttons1menu_screen/Buttons1MenuPresenter.hpp>
class Buttons1MenuView : public Buttons1MenuViewBase
{
public:
Buttons1MenuView();
virtual ~Buttons1MenuView() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void buttonRGOPressed();
// virtual void button2H1BPressed();
// virtual void button2H2BPressed();
virtual void scrollListUpdateItem(MenuItem& item, int16_t itemIndex);
virtual void scrollListItemSelectedCallbackHandler(const touchgfx::ScrollList&, int itemIndex);
void saveCurrentScreenIndex(int screenIndex)
{
presenter->saveCurrentScreenIndex(screenIndex);
}
int getCurrentScreenIndex()
{
return presenter->getCurrentScreenIndex();
}
protected:
touchgfx::Callback<Buttons1MenuView, const touchgfx::ScrollList&, int> itemSelectedCallback;
};
#endif // BUTTONS1MENUVIEW_HPP
Buttons1MenuView.cpp
#include <gui/buttons1menu_screen/Buttons1MenuView.hpp>
#include <gui_generated/common/FrontendApplicationBase.hpp>
#include "config_file.h"
#include "math.h"
static int8_t index_trig;
static int position;
Buttons1MenuView::Buttons1MenuView() : itemSelectedCallback(this, &Buttons1MenuView::scrollListItemSelectedCallbackHandler)
{
// Initialization code for ScrollList, if needed
}
void Buttons1MenuView::setupScreen()
{
Buttons1MenuViewBase::setupScreen();
saveCurrentScreenIndex(8);
}
void Buttons1MenuView::tearDownScreen()
{
Buttons1MenuViewBase::tearDownScreen();
}
void Buttons1MenuView::buttonRGOPressed()
{
// Override and implement this function in Buttons1Menu
if(textButtonRGO.isVisible())
{
//turn off
CONFIG.RGOMode[CONFIG.mode]=0;
textButtonRGO.setVisible(0);
}
else
{
CONFIG.RGOMode[CONFIG.mode]=1;
textButtonRGO.setVisible(1);
}
textButtonRGO.invalidate();
}
void Buttons1MenuView::scrollListUpdateItem(MenuItem& item, int16_t itemIndex)
{
if(itemIndex==0)
index_trig = itemIndex;
else if(itemIndex==1)
index_trig = itemIndex;
else if(itemIndex==2)
index_trig = itemIndex;
item.setWheelElements(itemIndex);
scrollList.invalidate();
index_trig = itemIndex;
}
void Buttons1MenuView::scrollListItemSelectedCallbackHandler(const touchgfx::ScrollList&, int itemIndex)
{
// Handle item selection here
position = itemIndex;
// Example: Update a text area with the selected item
// Unicode::snprintf(selectedItemTextBuffer, TEXT_BUFFER_SIZE, "Selected: %d", itemIndex);
// selectedItemText.invalidate();
}
2025-01-29 05:06 AM
Hello @FJB2069 ,
I'm not sure about the issue you're having. I've tried on my side to make an application similar to what you want to achieve (from what I understood). It works fine on my side. I'm sharing it here. Please let me know if this was what you wanted to achieve.
2025-01-29 08:07 AM
Thank you for your help!
I see that the <value> (0,1,2) is being updated correctly from ScrollWheel. I am not understanding how the ScrollWheel is sending the S1,S2,S3 index to the <value>? How is the Scrollwheel linked to textArea2?
2025-02-03 05:16 AM
Hello @FJB2069 ,
In Screen1View.cpp it is this function that updates the textArea's wildcard:
void Screen1View::scrollWheelAnimateToHandler(int16_t itemSelected)
{
Unicode::snprintf(textArea2Buffer, 3, "%d", itemSelected);
textArea2.invalidate();
}
Regards,
2025-02-03 07:14 AM
I missed that, thank you!
2025-02-03 08:23 AM
My pleasure! :smiling_face_with_smiling_eyes: