cancel
Showing results for 
Search instead for 
Did you mean: 

Screen starts to flicker when brightness is raised above a certain value

Emilmart
Senior

Hi everyone,

I can print nice pictures & transitions on the display of my custom board.

But when I'm rasing the brightness of the display (by setting the PWM backlight value), at a certain value the screen starts to flicker. Controls are shaking and if I continue to raise the brightness it flickers more.

Below that critical value it's working well, as you can see on the pictures joined.

0693W00000BaXYHQA3.jpg0693W00000BaXR7QAN.jpgI'm using a LCD TFT (parallel interface) with external SDRAM & TouchGFX.

What could cause this ?

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
Emilmart
Senior

solved, it was my input voltage that was dropping due to bad connectic

View solution in original post

2 REPLIES 2
Emilmart
Senior

solved, it was my input voltage that was dropping due to bad connectic

Good to hear it works, thanks for sharing :thumbs_up:

/Romain