2022-09-26 11:20 PM
Respected Sir/Mam , I cannot able use the keyboard example in the ongoing project of the same screen in STM32H7B3I-EVAL.When I have tried to insert it, it is not visible and having blank code inside it. Although Touch GFX 4.17 version has that facility.
Solved! Go to Solution.
2022-10-03 05:44 AM
Something must be wrong about your TouchGFX installation then.
When I download the Keyboard widget (Custom Container) we just made, import it into a blank project and run the application, it works first try for me.
What did you do exactly ?
Did you use the "Import Custom Container" feature of TouchGFX to call it into your project ?
/Yoann
2022-10-03 06:55 AM
Yes, we did exactly the same import the custom container with .tpkg extension. What will be the procedure after that? Do I need to add an instance of that container in my screen or using code need to add the container?
We've tried to add object of container in screen using the touchGFX designer but after that code does not building in STM32CubeIDE. Showing some errors.
2022-10-04 01:54 AM
Did you remember to generate code and select CubeIDE toolchain in CubeMX ?
/Yoann
2022-10-04 01:58 AM
Yes I have done it already but it has 37 errors in its base files which are read only and not able to edit.
2022-10-04 02:01 AM
I think you need to share your project at this point.
/Yoann
2022-10-04 02:23 AM
okay I will share it.
2022-10-04 02:39 AM
2022-10-06 02:09 AM
Hello I have sent you the project.