2025-03-10 7:51 PM
Hi,
as you can see in the first screenshot, in the X-CUBE-TOUCHGFX settings (TouchGFX Generator tab) the LTDC option for the Application Tick Source is not available. And at the bottom it says "LTDC in only available if enabled".
LTDC is enabled and configured (second screenshot). Does it need to be configured and/or enabled in some other ways or some other place too?
Thank you :)
2025-03-11 3:37 AM
Yes, in your first screenshot, under Display -> Interface, you have the change the value from Custom to LTDC.
2025-03-11 8:29 AM
Thank you @jchernus-fikst
but as you can see it is greyed out and cannot be selected. I was asking why and what else I would need to enable in order for it to not be greyed out so I can select it.
Thank you :)