2021-08-22 9:03 AM
Hello,
I have a button with a pause icon on it in TouchGFX, and I want to know how I can change the pause icon into a play icon after it is pressed. TouchGFX only gives me an option to change the icon while the icon is being pressed.
Solved! Go to Solution.
2021-08-24 9:18 AM
Thank you, so I was able to do the task by using the setBitmaps function. Here's the code I came up with:
if (OSC_Status.Running_Stat == Stopped) { //from pause to play:
OSC_Status.Running_Stat = Running;
RunButton.setBitmaps(touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_BLUE_ICONS_PAUSE_32_ID),
touchgfx::Bitmap(BITMAP_BLUE_ICONS_PAUSE_32_ID));
// don't forget to invalidate
} else { //from play to pause
OSC_Status.Running_Stat = Stopped;
RunButton.setBitmaps(touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_PLAY_32_ID),
touchgfx::Bitmap(BITMAP_PLAY_32_ID));
// don't forget to invalidate
}
also include "BitmapDatabase.hpp".
the bitmap id can be found in the images section of TouchGFX:
2021-08-23 7:02 AM
TouchGFX Designer can't do this for you, you must make code by yourself, fortunately, there is many demo can help us, for example demo "audio_player_screen", my board is STM32H747i-DSCO. the demo can download from github.
following code extact from "audio_player_screen":
ClickListener<Button> playButton;//in header of view Class, you should use ClickListener other than use Button directly
playButton.setAction(playCallback);//in Constructor
playButton.setClickAction(playTouchedCallback);//in Constructor
void AudioPlayerView::playButtonTouched(const Button&, const ClickEvent& evt)
{
coverImage.setTouched(evt.getType() == ClickEvent::PRESSED);
}
void AudioPlayerView::playButtonClicked(const AbstractButton& btn)
{
presenter->playPauseClicked();
playerState = presenter->isAudioPlaying() ? PLAYING : PAUSED;
if (playerState == PLAYING)
{
playButton.setBitmaps(Bitmap(BITMAP_PAUSE_BUTTON_ID), Bitmap(BITMAP_PAUSE_BUTTON_ID));
}
else
{
playButton.setBitmaps(Bitmap(BITMAP_PLAY_BUTTON_ID), Bitmap(BITMAP_PLAY_BUTTON_ID));
}
playButton.invalidate();
...
}
2021-08-24 9:18 AM
Thank you, so I was able to do the task by using the setBitmaps function. Here's the code I came up with:
if (OSC_Status.Running_Stat == Stopped) { //from pause to play:
OSC_Status.Running_Stat = Running;
RunButton.setBitmaps(touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_BLUE_ICONS_PAUSE_32_ID),
touchgfx::Bitmap(BITMAP_BLUE_ICONS_PAUSE_32_ID));
// don't forget to invalidate
} else { //from play to pause
OSC_Status.Running_Stat = Stopped;
RunButton.setBitmaps(touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_DARK_BUTTONS_SQUARE_ICON_BUTTON_ID),
touchgfx::Bitmap(BITMAP_PLAY_32_ID),
touchgfx::Bitmap(BITMAP_PLAY_32_ID));
// don't forget to invalidate
}
also include "BitmapDatabase.hpp".
the bitmap id can be found in the images section of TouchGFX: