2019-03-07 9:17 AM
I've done a quick search and could not see this mentioned hence...
I have two displays connected to my development computer. When editing a custom container if I move the TouchGFX designer from one display to another this can cause the widgets to be shifted relative to the container. Sometimes this needs this only happens if the designer is maximised.
The good news if that its just a display issue, flipping to canvas and back to containers fixes it, but it will give you a fright the first time.
2019-03-07 10:13 AM
I have two monitors too but it doesn't happen with me, but thanks for advice.
What I could expirience is adding a new font in windows, use some Text in TouchGFX and in the next day the font doesn't appear properly in the monitor, but in the demoboard appears correctly. I don't know the reason but in the end it works!
2019-03-08 12:51 AM
2019-03-08 2:55 AM
My monitors have the same resolution, 1920x1080 and 1080x1920.. maybe because this doesn't happen with me.
Regards.
2019-03-08 3:23 AM
2019-03-08 5:34 PM
If you could attach screen capturse of the issues you're seeing i'd be very interested.
Thanks!
2019-03-11 2:51 AM