2024-05-15 07:02 PM
I'm running the following git source on the NUCLEO-G071RB with NUCLEO-GFX01M2.
GitHub - lvgl/lv_port_stm_nucleo_g071rb: LVGL ported to ST's NUCLEO G071RB board
But, I got an error at the cursor location from the attached figure (LCD Error 1.png).
The return value of "data" from st7789v_recv_data function was all 0.
I'm not sure this is correct. I guess there should be some values in it.
When I run the X-Cube-Display sample program, I got the same error.
Please let me know what cause this kind of error.
Solved! Go to Solution.
2024-05-23 03:54 PM
Thank you for the Mohammad MORADI's advice.
I found an answer from https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/any-totally-working-sample-projects-for-nucleo-g071rb-x-nucleo/m-p/81867?search-action-id=21371795825&search-result-uid=81867.
Thanks,
2024-05-16 03:09 AM
Hello @jasonlee3 ,
I'm not sure if you are planning on using graphics on your board or not, but I suggest using TouchGFX instead of your current project.
TouchGFX has already a Board Setup which contains all the required settings for NUCLEO-G071RB + GFX01M2; You just need to develop your GUI and the rest in handled by TouchGFX.
TouchGFX Board Setup for NUCLEO-G071RB
I hope this helps you, don't hesitate to ask more questions
2024-05-23 03:54 PM
Thank you for the Mohammad MORADI's advice.
I found an answer from https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/any-totally-working-sample-projects-for-nucleo-g071rb-x-nucleo/m-p/81867?search-action-id=21371795825&search-result-uid=81867.
Thanks,
2024-05-24 01:12 AM
Glad to hear you found a solution!
You're very welcome and good luck