2020-10-14 8:53 AM
I have a NUCLEO-G071RB with X-NUCLEO-GFX01M1 display board and I've imported the GFX01M1_HelloWorld application but it won't launch into debug. I get this error:
Error in final launch sequence:
Failed to execute MI command:
load /Users/sukkinpang/STM32CubeIDE/workspace_stm32g0_imported/Projects/NUCLEO-G071RB/Applications/GFX01M1_HelloWorld/STM32CubeIDE/Debug/X-NUCLEO-GFX01M1.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /Users/sukkinpang/STM32CubeIDE/workspace_stm32g0_imported/Projects/NUCLEO-G071RB/Applications/GFX01M1_HelloWorld/STM32CubeIDE/Debug/X-NUCLEO-GFX01M1.elf
How can I fix this ?
Solved! Go to Solution.
2020-10-16 1:16 AM
HI please refer to this post. https://community.st.com/s/question/0D53W00000LC29WSAT/important-working-on-the-stm32g0-nucleo-with-stm32cubeide
It is a new step necessary for the G0 and upcoming new ST kits.
2020-10-14 10:31 PM
Hello,
Instead of doing this, can you try the G071-NUCLEO Application Template available in the Designer and do a simple GUI with a box and a button ?
This Application template was done by TouchGFX but not the GFX01M1_HelloWorld.
/Alexandre
2020-10-15 3:14 AM
Hi Alexandre,
I've started Designer but there is no template for the G071-NUCLEO.
How do I get this template ?
Sukkin
2020-10-15 3:52 AM
Hi,
Are you using TouchGFX 4.15 ? The STM32G0 nucleo application template is only available in this new version.
FYI I will create a new post on the forum to explain how to work with STM32CubeIDE and the G0 (you can still run your project on target from Designer with no issue) if this your case as well. Unlike all of the other boards this AT requires to manually add the external loader to the installation folder of CubeIDE in order to be able to debug and run the project. Building is already working fine without this.
/Romain
2020-10-15 8:23 AM
Where can I get 4.15 ?
The download is only shows 4.14.
2020-10-15 1:55 PM
Managed to install Designer 4.15 and got a button and new screen working on the simulator. Generated the code.
In CubeIDE used Open project from file system and it compiled ok but when I tried to upload the code I get this error:
ERROR: Couldn't parse external memory loader 'S25FL032P_STM32G071B-NUCLEO.stldr'
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (-2147155971) Unknown. Please check power and cabling to target.
In the Debugger setting the External Loader is checked and this is selected:
S25FL032P_STM32G071B-NUCLEO, 0x90000000, SPI_FLASH, S25FL032P_STM32G071B-NUCLEO.stldr
Then in CudeIDE I've created a test program and it uploaded to the board and ran ok, so I know the hardware is work.
Any idea of how to fix this ERROR: Couldn't parse external memory loader 'S25FL032P_STM32G071B-NUCLEO.stldr' ?
2020-10-15 2:00 PM
In Designer I also clicked Run Target but I get this error:
Compiling TouchGFX/App/app_touchgfx.c
Compiling gcc/syscalls.c
Compiling gcc/sysmem.c
Compiling ASM gcc/startup_stm32g071rbtx.s
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
Done
Flash
make -f ../gcc/Makefile flash
Reading TouchGFX/application.config
Linking TouchGFX/build/bin/target.elf
Producing additional output formats...
target.hex - Combined internal+external hex
intflash.elf - Internal flash, elf debug
intflash.hex - Internal flash, hex
extflash.bin - External flash, binary
/usr/bin/sh: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe: No such file or directory
gcc/Makefile:260: recipe for target '_extflash_' failed
make[1]: *** [_extflash_] Error 127
../gcc/Makefile:47: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
Failed
Do I have to install the STM32_Programmer_CLI.exe myself ?
2020-10-15 10:06 PM
It seems you haven't installed STM32CubeProgrammer.
Please install it, the CLI is automatically installed along with it.
CubeProgrammer is mandatory to be able to flash STM32 boards.
/Alexandre
2020-10-16 1:07 AM
Ok, I've now installed STM32CubeProgrammer and when I click Run Target the code is uploaded and I can see buttons on the LCD. Great !!
I then tried to debug the program in CubeIDE but still get the error:
ERROR: Couldn't parse external memory loader 'S25FL032P_STM32G071B-NUCLEO.stldr'
Any ideas ?
2020-10-16 1:16 AM
HI please refer to this post. https://community.st.com/s/question/0D53W00000LC29WSAT/important-working-on-the-stm32g0-nucleo-with-stm32cubeide
It is a new step necessary for the G0 and upcoming new ST kits.