cancel
Showing results for 
Search instead for 
Did you mean: 

nucleo-g071rb + example touchGfx designer 4.1.16

BTeof.1
Associate

I’m trying to run the example of touchgfx stm32g071 nucleo demo, but when I import to stm32ide and debug, the program never returns from the function "void tick" in " HAL::getInstance()->backPorchExited() or do I need to change the code somewhere?

thank you.

1 REPLY 1
Yoann KLEIN
ST Employee

Hello @BTeof.1​ ,

If I understand correctly, you are using TouchGFX 4.16 ?

If yes, could you please upgrade to 4.20 and see if there is still compilation errors ?

Thank you,

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX