2024-11-27 12:30 AM
Hello,
I am currently working with the TouchGFX Designer tool and have successfully created a simulator project. I would now like to migrate this project to the STM32H7S78-DK board but am unsure of the necessary steps or adjustments required.
Could you please guide me through the migration process?
Board: STM32H7S78-DK
TouchGFX Version: 4.21.1
IDE: STM32CubeIDE
Thank you!
Mehul
Solved! Go to Solution.
2024-11-27 6:12 AM
Hello @Mehulrana511
To migrate the project, you can use the "Import GUI' option in the "Edit" tab in Designer:
Click the "Import GUI" button to open the Import GUI window. Then, click the "Browse" button allowing for selection of a TouchGFX Designer project (.touchgfx) to be imported into the current project.
Please follow the steps in this TouchGFX guidelines.
2024-11-27 6:12 AM
Hello @Mehulrana511
To migrate the project, you can use the "Import GUI' option in the "Edit" tab in Designer:
Click the "Import GUI" button to open the Import GUI window. Then, click the "Browse" button allowing for selection of a TouchGFX Designer project (.touchgfx) to be imported into the current project.
Please follow the steps in this TouchGFX guidelines.
2024-12-19 6:25 AM - edited 2024-12-19 7:25 AM
Hi,
I have successfully migrant simulator project to STM32H7S78-DK board,
but after migration load and simulator option is disabled.
Here i attached screenshot,
/Mehul