cancel
Showing results for 
Search instead for 
Did you mean: 

LTDC generation code issue

MSale.1
Senior

Hi,

some thing is strange with the cube ide in the display controller LTDC initialization . i choose 1 layer only but the cube ide generate code for 2 layers!!

First time to see such thing

1 ACCEPTED SOLUTION

Accepted Solutions

As a workaround , you need to delete the unnecessary code (the wrong config of the unused layer).

Regards,

Khouloud

View solution in original post

9 REPLIES 9
Khouloud ZEMMELI
ST Employee

Hi @Community member​ 

Could You please share you ioc file ?

Regards,

Khouloud

0693W000005AUXfQAO.png0693W000005AUXoQAO.png0693W000005AUXeQAO.png

@Khouloud ZEMMELI​ 

Hi,

Also there is problem with the touchgfx it does not set the resolution correctly always fixed at 800 * 480 and also the CUBE ide look change as you see in the photo0693W000005AUaOQAW.png0693W000005AUaJQAW.png0693W000005AUaEQAW.png

TWard.1
Associate II

I have the exact same issue, and I'm concerned its affecting performance.

Can anyone help?

Hi @TWard.1​ 

Need to know the part number used, the config and the tool version or it will be more better if you share your ioc file.

Thanks

Khouloud

TWard.1
Associate II

sorry my bad.

Thanks @TWard.1​ 

@Community member​ & @TWard.1​ : Issue confirmed and now fixed, the fix will available for the next CubeIDE/MX release (1.5.0 - 6.1.0 ) which will be W47/48.

We are deeply sorry for any inconvenience this may have caused.

Best Regards,

Khouloud

TWard.1
Associate II

what is the impact and the workaround? It seems that this is causing my double buffering to not work properly and write to the other layer?

As a workaround , you need to delete the unnecessary code (the wrong config of the unused layer).

Regards,

Khouloud