2020-08-26 09:54 AM
Hello friends
My problem is I can not widgets load to 25q256 via qspi I do not know what the problem is in my program, I put the project for you to find the problem, thanks
2020-09-04 09:09 PM
Thank you very much if possible a sample code for me with the software keil or cubeide for stm32h743
2020-09-05 02:51 AM
If you're going to use CubeIDE: latest version comes with OpenOCD with stmqspi driver for external NOR flash built in. All you'd have do is to adjust ist the pin initialization (for proper AF setting) and the flash initialization. For that a good starting point is:
http://openocd.zylin.com/#/c/4321/7..9/tcl/board/nucleo-h743zi.cfg
Unfortunately ST had squeezed the setups for various disco boards into the single file stm32h7x.cfg ... So the stuff related to the disco boards has to be replaced by the config for your board. Would have been easier if ST had kept separate file for each board :(
2020-09-05 07:01 AM
Thank you very much for your help, but I did not understand how to file .stldr To make my own schematic of the board
2020-09-05 07:05 AM
What do you think about this?
https://blog.naver.com/PostView.nhn?blogId=chcbaram&logNo=221785788076
2020-09-06 05:29 PM
Looks like a good starting point, you'll need to adapt to support the 25Q256 part
2020-09-08 07:57 PM
External loader for W25Q256FV on CUSTOM (HSE:25 MHz, CS:PB6:AF10, CLK:PB2:AF9, D0:PE8:AF10, D1:PE9:AF10, D2:PE7:AF9, D3:PE6:AF9)
Note still some buggy behaviour with STM32 Cube Programmer v2.5.0, might need to Disconnect-Connect ST-LINK for the external loader Init function to be called properly. See: https://community.st.com/s/question/0D50X0000BRWFmKSQX/stm32-cube-programmer-v210-not-working-with-stm32h750bdk-qspi-external-loader
PayPal or Amazon Gift Cards to sourcer32@gmail.com
2020-09-10 02:58 AM
True, but it's not clear how to create a file stldr
2020-09-10 06:40 AM
Ok, but it is a small .ELF object, much like a DLL, which is loaded into RAM and accessed via a number of exported functions.
It doesn't have a main.c or main() entry point.
Basically the Dev_inf.c / Loader_Src.c, BSP code to support the QSPI device, and HAL library files to support the hardware used.
Posted a .STLDR for the W25Q256 earlier in the thread, yesterday.
2020-09-10 08:29 AM
Thank you very much. Can you put the address of that post?
2020-09-10 11:42 AM
Comes up as the last post on the first page of this thread.
This Salesforce forum software lacks the ability to cite a specific post in a specific thread. Or index posts from a specific users.
#DefectiveByDesign