cancel
Showing results for 
Search instead for 
Did you mean: 

L8_RGB565 images issue

TDele.1
Associate III

Hello,

To save space on the section "ExtFlashSection" with the dev board STM32F469I-DISCO, I'm trying to use the L8_RGB565 format for my backgrounds. I'm doing this by changing the "Image Format" of all background on the "Images" section of TouchGFX Designer. This is working when I launch the Simulator but when I try actually seeing it on the board, the colors are weird like so:

Simulator:

0693W00000ANZGtQAP.pngSTM32F469I-DISCO:

0693W00000ANZHwQAP.pngHow can I solve the issue ?

Thanks in advance,

DELETRAZ Tristan

10 REPLIES 10

Starting over the project with an older version is never fun but if it can solve the issue then this option could be considered (otherwise this should be fixed in TouchGFX 4.17 but there are no estimated release date yet)