cancel
Showing results for 
Search instead for 
Did you mean: 

Issue: When adding new image to assets it appears as directory in TouchGFX Designer

ypiotrp
Senior

Hello,

I found a bug or maybe a feature 

When I add a new image to assets/images directory in my project it appears in the TouchGFX Designer but I cannot use it. It is so because it is shown as a direcotry, not an image file. Sometimes using Generate Code helps with that, sometimes I have to choose another image and when I again try to choose the new one it shows up as an image, not directory. Below you can see a screenshot showing this issue:


_legacyfs_online_stmicro_images_0693W00000bkM7dQAE.png 

Regards,

Piotr

2 REPLIES 2
Yoann KLEIN
ST Employee

Hello @Community member​,

Which version of TouchGFX are you using?

I'm personally using 4.21.4 and I'm not able to reproduce this bug.

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX
ypiotrp
Senior

Hi,

I'm using TouchGFX 4.20. Could it be that this bug has been already fixed in the newest version? I haven't seen such a description in release notes.

Regards,

Piotr