2019-05-27 4:30 AM
Hi All,
When I tested this example, I made one change is to use Circular and the error is showed below:
Seems the item not match, can you help me to fixed it, thanks very much.
2019-05-27 4:34 AM
Hi @Redifinition,
Did you mean to attach something? Maybe you were fooled by this editor into thinking that you could paste a screenshot in because it actually shows up. It won't make it to the final post unfortunately.
/Martin
2019-05-27 5:31 AM
Thanks, Martin.
2019-06-11 1:04 AM
Hi,
Could you send me the project? the "?" indicates a fall back character because we could not locate the proper glyphs in the specified font.
/Martin
2019-06-11 5:22 PM
2019-06-11 5:22 PM
2019-06-12 12:21 AM
Hi again,
Thanks. I'll check when i can. Is this application based solely on the example from the designer? If so that definitely looks like there's an error!
/Martin
2019-06-12 10:51 PM
The example from the designer does not behave that way when making the wheel circular. Hmm. I am, however, seeing some weird fallback character issues when at the last element in the list. You posted a similar issue near the beginning of the post.
2019-06-13 7:22 AM
the project is from designer
2019-06-13 4:07 PM
Okay, strange that we're seeing different behaviors. You did nothing other than make the wheel circular?