cancel
Showing results for 
Search instead for 
Did you mean: 

IS there a graphics engine for STM32H475 available?

Hansel
Senior

Hi, I'm new to this board. I've decided to switch from ATMEL to STM µControllers after Microchip bought ATMEL and apparently decided to phase out ATMEL Studio.

I bought the STM32H745 Discovery board assuming TouchGFX would be working on it. However, after downloading the software package, it says that this MCU doesn't support TouchGFX. Is there an alternative graphics engine available? Or do I have to return the demo board for a different one that allows me to prototype for use with LTDC on an RGB interface?

3 REPLIES 3
MM..1
Chief III

Hxxx i mean support it , but MX wizard project mode isnt prepared. You need create project manualy or use TouchGFX prepared.

Hansel
Senior

That's what I was afraid of, but thanks for confirming. Plowing through the documentation now...

You choice Ferrari and have driver licence for automat :beaming_face_with_smiling_eyes: