2022-10-02 10:19 AM
I have a new project with TouchGFX and currently create a huge bunch of new screens.
As I have my own set of images (.png) for buttons etc. I do not use the integrated skins.
When placing a radio button or checkbox now with my own images, it is very time consuming to select the images for e.g. 4 states of a radio button from my own set of images.
My question therefore: Is it possible to create a customized skin so that I can select my preset skin images for the standard checkboxes and progress buttons etc?
This would speed up the creation of setup menus dramatically!
I could not find such a feature.
Solved! Go to Solution.
2022-10-03 01:40 AM
Hi GS@S,
Yes It's possible :)
Here's how you can do it :
1- Go to your TouchGFX installation path, and navigate to this folder : "TouchGFX\4.20.0\designer\Skins"
2- Copy paste one of the Folder already there, for example "Blue", and rename you new folder with the name you want for your own customized skin :
3- Open you new folder, and edit the skin.json file. You'll see on the first line, an entry called "Name". Replace the value with your new skin name :
{
"Name": "Own_customized_skin",
...
}
4- Replace all the images you need in each of the folders
Be careful, TouchGFX Designer will warn you if the image you've put doesn't suit, for example, for check_buttons, all of the buttons need to have same size.
6- If you need to rename the images, edit again the skin.json file to add/rename an image. You'll probably also need to edit it if your image has other dimensions than the one you replace.
Hope it helps.
/Osman
2022-10-03 01:40 AM
Hi GS@S,
Yes It's possible :)
Here's how you can do it :
1- Go to your TouchGFX installation path, and navigate to this folder : "TouchGFX\4.20.0\designer\Skins"
2- Copy paste one of the Folder already there, for example "Blue", and rename you new folder with the name you want for your own customized skin :
3- Open you new folder, and edit the skin.json file. You'll see on the first line, an entry called "Name". Replace the value with your new skin name :
{
"Name": "Own_customized_skin",
...
}
4- Replace all the images you need in each of the folders
Be careful, TouchGFX Designer will warn you if the image you've put doesn't suit, for example, for check_buttons, all of the buttons need to have same size.
6- If you need to rename the images, edit again the skin.json file to add/rename an image. You'll probably also need to edit it if your image has other dimensions than the one you replace.
Hope it helps.
/Osman
2022-10-03 03:40 AM
Wow! Thank you for this information. Will help a lot!
BR GS
2022-10-03 04:27 AM
You're welcome!