2023-09-10 03:26 AM
I have been trying to display continuous data on Scroll wheel container for the past 2 months but have been very unsuccessful. Could someone help or tell me if it's even possible to do that?? The example in the documentation does not help in that regard.
I would like to display a counter that goes from 0 to 255 on a scroll wheel but what I get is the exact same value on each row of the scroll updating in real time. What I want is each counter value displayed on each row, e.g
This is my customContainer setup:
void CustomContainer2::RX_UART(char* data)
{
TX_BufferArea.setWideTextAction(touchgfx::WIDE_TEXT_WORDWRAP);
sprintf(USART_Array, "%d", data);
Unicode::strncpy(TX_BufferAreaBuffer, USART_Array, TX_BUFFERAREA_SIZE);
TX_BufferArea.invalidate();
}
This is displayed via the View:
void Screen2View::scrollWheel2UpdateItem(CustomContainer2& item, int16_t itemIndex)
{
item.RX_UART((char*)CounterTimer); //I feel itemIndex should be somehow added to this line here but I don't know how to do that codewise...Please help!!
int indexOfitemAtTopOfTheList = scrollWheel2.getSelectedItem();
scrollWheel2.animateToItem(indexOfitemAtTopOfTheList + 1);
}
In the main:
volatile uint8_t CounterTimer = 0;
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
if(htim->Instance == TIM2)
{
CounterTimer++; //Incremented every 1 second
}
}
Solved! Go to Solution.
2023-09-10 04:03 PM
Hello @Krautermann ,
I created a small example you can get inspiration from. I started from the "Scroll Wheel and List example" from TouchGFX Designer and I removed the "List" part. Then I added a handleTickEvent for the counter and made the wheel animate each 60 ticks. You'll find my project in attachment.
Hope it helps 😉
2023-09-10 04:03 PM
Hello @Krautermann ,
I created a small example you can get inspiration from. I started from the "Scroll Wheel and List example" from TouchGFX Designer and I removed the "List" part. Then I added a handleTickEvent for the counter and made the wheel animate each 60 ticks. You'll find my project in attachment.
Hope it helps 😉
2023-09-19 05:37 AM
Solution provided accepted after several days of testing.
Although user needs to modify it according to his application. Here is my modified code if anyone is interested:
void Screen2View::handleTickEvent()
{
if(tick%1==0)
{
snprintf(ActualBuffer, sizeof(ActualBuffer), "%s", (char*)currentBuffer);
if (strcmp(ActualBuffer, PreviousBuffer)!=0)
{
snprintf(temporaryBuffer, sizeof(temporaryBuffer), "%s", (char*)currentBuffer);
scrollWheel1.animateToItem(scrollWheel1.getSelectedItem()-1);
flag2Scroll1 = 1;
snprintf(PreviousBuffer, sizeof(PreviousBuffer), "%s", ActualBuffer);
}
int currentCounterTimer = CounterTimer;
if (currentCounterTimer != previousCounterTimer)
{
flag2Scroll2 = 1;
scrollWheel2.animateToItem(scrollWheel2.getSelectedItem()-1);
previousCounterTimer = currentCounterTimer;
}
}
}
void Screen2View::scrollWheel1UpdateItem(CustomContainer1& item, int16_t itemIndex)
{
if(flag2Scroll1==1)
{
item.RX_SPI((char*)temporaryBuffer);
flag2Scroll1 = 0;
}
}
void Screen2View::scrollWheel2UpdateItem(CustomContainer2& item, int16_t itemIndex)
{
if(flag2Scroll2==1)
{
item.RX_UART((char*)TX_Buffer4);
flag2Scroll2 = 0;
}
}