2019-01-28 1:07 AM
In my case,intermediately TouchGFX evaluation watermark is shown on screen.And i have programmed application for STM32L4R5 board.
Are we need to obtain a licensed version of the TouchGFX library.
If this is the case then,How to obtain a licensed version of the TouchGFX library?
2019-01-28 1:13 AM
Hi @ABhan,
Since 4.10.0 there is no longer any watermark. Instead, TouchGFX is locked to STM32. No licenses required!
Hope that helps,
Best regards,
Martin
2019-01-28 1:19 AM
Thank you Martin.
Then Why my application showing watermark on STM32L4R5 nuclio board application?
2019-01-28 1:21 AM
Hi Atul,
Which version of TouchGFX are you running? If you downloaded 4.10.0 from the ST website the watermark should not be there.
2019-01-28 2:36 PM
Can you please double check? I'd be very interested to hear back. The watermark code is completely removed from the framework since 4.10.0 (The first release after ST acquisition) so it should definitely not be there. I think you're the first to report this, also, so i'm hoping you just have a pre-ST version.
Best regards,
Martin