2020-09-24 2:22 AM
I have asked this question before and got no answer from STM so its better to clear it for us so we know
2020-09-24 3:34 AM
Hello @Community member ,
According to the STM32H743 datahseet: max clock for DCMI is 80MHz. this data is the result of characterization.
Hope this answer your question.
Please select the post as a "Best Answer" if it answers your question.
Thanks
Imen
2020-09-24 3:43 AM
@Imen DAHMEN
Hi
In the datasheet its mentioned 80Mhz at 400Mhz. so even at 480Mhz the max will still be 80Mhz or 96Mhz?
2020-09-24 6:28 AM
The reference manual says on page 1187 (DCMI Clocks): "The maximum DCMI_PIXCLK period must be higher than 2.5 HCLK periods."
So, if AHB clock is 240 MHz / 96Mhz = 2.5
Maybe is possible to work, but you are trying to use the DCMI interface in the max clock possible. I don't know if is a good ideia!
Best Regards,
Kunde