2020-11-10 09:57 PM
Thank you for helping.
environment:
board: STM32F769I-DISCO
TouchGFX 4.15.0
Is it possible to set COLOR DEPTH to 24 Bit?
If you can't, please tell me the reason.
Thank you.
Solved! Go to Solution.
2020-11-11 05:50 AM
Try following the reverse of the procedure outlined in comments of this post. YMMV.
If you are starting a new project, you can just use the 3.0.1 template, which uses 24bpp by default.
2020-11-11 05:50 AM
Try following the reverse of the procedure outlined in comments of this post. YMMV.
If you are starting a new project, you can just use the 3.0.1 template, which uses 24bpp by default.
2020-11-12 08:15 PM
Thank you for your reply.
I was able to realize it.
2020-11-13 09:35 AM
You're welcome. Did you follow the reverse procedure or did you use the 3.0.1 template?