cancel
Showing results for 
Search instead for 
Did you mean: 

I think there is a bug in the STM32CubeIDE Version: 1.4.0 Build: 7511_20200720_0928 (UTC), section “device configuration tool�?, section STMicroelectronics.X-CUBE-TOUCHGFX.4.15.0 Mode and configuration.

AGendrau
Associate

When Graphics Application is checked, a folders tree starting from TouchGFX, with files like GFX2.touchgfx, etc, is generated. It’s OK.

When the .ioc file becomes complicated (as the example I attach), it seems that TouchGFX is replaced by Src and all files are generated under Src, mixing them with main.c and the other files.

Could you fix this, please?

2 REPLIES 2
Martin KJELDSEN
Chief III

Can you elaborate on what you mean by "complicated" ? And in this case do you mean that "TouchGFX" files are being put under "Src" ?

/Martin

Hello,
Elaborating on the question, I discovered that the problem with folders started after migrating from an old version.
I upgraded the STM32CubeIDE, and after I double clicked the .ioc file.
It appears this dialog. I choice ‘Migrate’.
[cid:image001.png@01D6BD82.458FF9F0]
I suppose that starting from scratch folders were OK.
Do you have a work-around?
Best regards.