2020-06-16 3:19 AM
I have doubt that the bandwidth of the internal memory which is 1536MB/s is too fast. i am using stm32h743 at 480 MHz and the AXI bus speed is 240MHz.
2020-06-24 3:27 AM
So if it's not supported you need to create your own external loader.
To do so, you can refer to this document https://www.st.com/resource/en/user_manual/dm00403500-stm32cubeprogrammer-software-description-stmicroelectronics.pdf Section 2.3.3.
I believe what's written for TrueSTUDIO is the same for CubeIDE.
/Alexandre
2020-06-24 3:52 AM
@Alexandre RENOUX
Thank you very much
Mahmoud