2019-07-12 3:00 AM
I managed to compile a project without error s but every time i flash it the display become black.
2019-07-12 4:40 AM
Hi @Community member,
Is your application running? Are you in a hardfault? Let us know!
/Martin
2019-07-12 5:56 AM
Hi,
Yes its in hardfault.exactly at MX_QSPI_Init.
Mahmoud
2019-07-15 12:34 AM
Hi @Community member
It could be that the configuration for QSPI is not correctly set up, have you done the configuration or have you used a template as a starting point? e.g. the Application Template from TouchGFX Designer?
/Anders
2019-07-15 4:20 AM
Hi @Anders Nedergaard PETERSEN
I solved the QSPI problem. i never tried to use the template but i just tried it now and when i open the IOC file with the cube ide i got this message "Invalid Input: Must be IFileEditorInput"
Mahmoud
2019-07-15 4:52 AM
@Community member , thank you for reporting this.
Please elaborate on the steps you performed when getting this error.
I guess you could work around this error, by opening the .ioc file with CubeMX and then in project settings select CubeIDE as the target IDE.
Great that you have found a solution for the QSPI issue!
/Anders
2019-07-16 2:24 AM
I followed the steps from your online video on how to integrate STM32f746G with cubeide on youtube and modified the configuration using the informations for my stm32f769 board from your website touchgfx.zendesk. after debugging i am stuck in DSI_IO_WriteCmd(2,lcdregdata2) which is inside MX_DS_Init() which is from OTM8009a_Init().
when i use template i end up with multiple errors.
Mahmoud
2019-07-18 3:18 AM
@Anders Nedergaard PETERSEN
Hi, i managed to integrate the touchgfx with the Cubeide and its working but now i have another problem that the touch does not work. i followed your video that solve this problem for the 746g board but for me it gave me error in the utilities files.
Mahmoud
2019-07-18 11:31 PM
Please have a look at this guide on how to add the BSP files to the STM32F769 disco board: https://touchgfx.zendesk.com/hc/en-us/articles/360020208091-Configuring-STM32F769I-DISCO
/Anders
2019-07-19 12:40 AM
@Anders Nedergaard PETERSEN
Thanks i managed to make it work yesterday. every thing is totally fine now. by the way touch gfx is really very promising tool.
Mahmoud