2022-07-25 05:03 AM
Hi everyone
I,m having a problem when i try to capture a photo in raw format with the OV5640 camera. I get an image of a suitable size but it adds the header of the JPEG that i want to avoid it.
When i try to open it with the image viewer, i can see the image but it has wrong colors.
I,m using ADC with DMA in Snapshot and when i starting the DCMI i have JPEGMode = DMI_JPEG_DISABLE
anyone can help me?
Thank you in advance
2022-07-25 05:06 AM
Pretty sure that information is coming from the camera, check what settings are in that, not the STM32