2019-11-14 3:04 AM
I follow the website https://touchgfx.zendesk.com/hc/en-us/articles/360024979552-Using-Binary-Fonts-and-the-Font-Cache. But i can not create any binary fonts. The app.mk is like that :
# Relative location of the TouchGFX framework from root of application
touchgfx_path := ../../Middlewares/ST/TouchGFX/touchgfx
# Optional additional compiler flags
user_cflags := -DUSE_BPP=16
# Settings for image converter output format
alpha_dither := yes
# Dither algorithms: 0 (no dither), 1 (Floyd-Steinberg), 2 (Jarvis, Judice and Ninke), 3 (Stucki)
dither_algorithm := 2
opaque_image_format := RGB565
non_opaque_image_format := ARGB8888
# Settings for image converter screen orientation (empty string =
# default value, -rotate90 rotates the image 90 degrees)
screen_orientation :=
# Settings for Hardware accelerated text rendering on STM32F4 and F7
# devices. Must correspond to value of bitsPerPixel for font to have
# any effect. If A4 blitcap is enabled for target specific HAL the
# fontconverter must generate compliant data format, otherwise
# resulting in a DMA Controller Configuration Error.
text_data_format := A4
# Setting for the textconverter. Identical texts across all languages
# are mapped to the same memory region to save internal flash memory
remap_identical_texts := no
# Location of the TouchGFX Environment
touchgfx_env := G:/TouchGFX/4.12.3/env
text_converter_options := remap A4 binary_fonts
Who can tell me what went wrong.Or give me a specific example.
Thank you very much.
2019-11-19 1:38 AM
Check the TouchGFX folder?
/Martin