cancel
Showing results for 
Search instead for 
Did you mean: 

I am using TouchGfx on STM32H747I-DISCO board. My final binay size is 2.13 GB

shiv50084
Associate

Default Image Configuation setting is :

shiv50084_0-1725195872774.png

Framework Features:

shiv50084_1-1725196429404.png

Size of .bin file 

shiv50084_2-1725196553300.png

Touch Gfx setting in IOC file:

shiv50084_3-1725196672067.png

 

I also followed the link:

https://community.st.com/t5/stm32-mcus-products/generated-binary-file-size-is-too-large-2-3gb/td-p/300719

 

But still size is 2.13 GB.

 

Can you please help me to reduce the size of binary?

@UtkrantiYantra 

 

 

6 REPLIES 6

Don't use a .BIN to describe two regions with large separation within the ARM's 4GB address space.

Use a .HEX, or divide into two or more .BINs describing the 0x08000000 and 0x90000000 regions separately.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MM..1
Chief II

In project settings uncheck bin file create.... you have hex ok.

@Tesla DeLorean 

I am using this command 

arm-none-eabi-objcopy.exe -O binary --only-section=ExtFlashSection "${BuildArtifactFileBaseName}.elf" ExtFlash.bin;arm-none-eabi-objcopy.exe -O binary --remove-section=ExtFlashSection "${BuildArtifactFileBaseName}.elf" STM32F746.bin

 

From mentioned link in query.

 

I need bin file for FPU. How can I create different  file from hex?

I don't expect the functionality of objcopy has changed. Review the command documentation and man page.

Check you're using the same/correct naming for the sections in the .ELF file. Check the .LD and what's described in the .MAP file

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
GaetanGodart
ST Employee

Hello @shiv50084 ,

 

We made a video about reducing flash size : How to TouchGFX: Save flash memory 

You could also check your compiler setting to reduce size (-Os for size optimization in GCC).

 

I hope this helps.
If this comment or another one solved your problem, I invite you to select it as "best answer".

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Hello @shiv50084 ,

Have you been able to solve your problem?
If so, I invite you to select the comment that helped you the most as "best answer".

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)