cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32F446RTE (64pins) with TouchGFX 4.18. The screen is working but there is slight flickering (slow refresh time). As I don't need touch screen function, can I stop continuous refreshing of the screen and only update the screen where needed.

RBoud.1
Associate II
 
2 REPLIES 2
MM..1
Chief III

touch screen function isnt relevant to this

yes if you have display with memory

RBoud.1
Associate II

Excellent, thank you. uController has 512KB flash and 128KB Ram. Program mem usage is Program Size: Code=140840 RO-data=96468 RW-data=580 ZI-data=46596. TouchGFX use partial mode. How can I achieve this or which TouchGFX function to call to refresh the screen? I Want to use flags to call this function.