2018-12-29 12:27 PM
ST's Appnote AN4861 (DM00287603), para. 4.5.1, "Memory Allocation" discusses "Splitting up the slave memories between masters...."
My StemWin application uses a single layer, with multi-buffering ("Front buffer" and "Back buffer"). I am able to set up the LTDC to switch between buffers located at pretty much any address I choose, but StemWin seems determined to choose it's own "Back buffer" address based on the setting of LCD_LAYER0_FRAME_BUFFER + (X size * Y size * Bytes per Pixel).
My question is: How can I configure StemWin to write to a specific, user-selected address for "Front Buffer", and a separate,
non-contiguous address for "Back buffer"? I understand there is a function to accomplish this when using the HAL, but I see no corresponding functionality when using StemWin.
Thanks,
Ron