2021-05-13 01:25 AM
Due to lots of image files for UI, I need to spend around 3~4 minutes programming the external flash. Can I specify a code area and an image area for the extenal flash? Then if image files are not changed, can I just update the code area?
Or is there any way to shorten the programming flash time for a project with TouchGFX?